What is the function of the 2 Switches located at the rear panel of SU3000RMX93_Shipboard

Question: What is the function of the 2 Switches located at the rear panel of SU3000RMX93_Shipboard

Product line: SU3000RMX93
Switches (toggle and rocker) at the back of the UPS are not properly labeled (no identification) and no information indicated on the product data sheet or no user's manual been uploaded/updated to our website which will cause the customer to be confused.

Environment: All Serial Numbers

Answer: (see below)

The said two switches refer to:

  1. Toggle Switch = Input enable/breaker switch (helps to provide overload protection).
  2. Rocker Switch =Enable Switch (simply enables or disables input power). Note: The said switch must be set to ON before turning the UPS.
See actual image:
Actual switch rear

Kindly do refer to the latest offer with the same switches (SMX3000RMX93). See link below:
https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=SU_UM-990-6473_EN.pdf&p_Doc_Ref=SPD_SU-UM-990-6473_EN
Rear Label

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: