How to fix the error " inconsistency detected in one or more DFBs" in CEV15.3 ?
With CE V15.3, a new message in the error window will appear : "Inconsistency detected in one or more DFBs"

To correct the issue :
1- Do an export of the "Derived FB Type"
2- Import back the "Derived FB Type"
3- A pop up opens called "Import Trouble Report" , select "Replace All":
ReplaceAll,DFB,Import
4. Build and save the application.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: