How do I password protect a section in my EcoStruxure Machine Expert HVAC M172 project?


Issue:
Password protecting a section in EcoStruxure Machine Expert HVAC M172 project


Product Line:
EcoStruxure Machine Expert HVAC, M172


Resolution:
To passwordprotect a POU section, select the POU from the project tree, right-click, then select Crypt in the context menu
m172_1

Enter the password and confirm the operation.
image



You will notice a key symbol next to the POU. This indicate that the POU is read/write protected.
image3

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: