Issue:
How can I download new application to M580 safety if I lost the password of current PLC ?
Product Line:
M580 SAFETY
Environment:
EcoStruxure Control Expert
Resolution:
User could swap the M580 safety CPU and copro and power up ,CPU will enter NO CONF status and user could download the new application via USB cable .
The CPU and Copro should be placed to normal position once application download.
Đã phát hành cho:Schneider Electric Việt Nam