Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
        
Hôm nay chúng tôi có thể giúp gì cho bạn?
Deployment of Data Center Expert 7.9.x VM only allows up to 8 CPU cores.
Issue:
Deployment of Data Center Expert 7.9.x only allows up to 8 CPU cores.

Product Line:
Data Center Expert

Environment:
DCE potentially any version
AP94VMACT deployment on VMware ESXI

Cause:
Data Center Expert VM was only built with the maximum capacity of 8 CPU cores. This was due to compatibility with ESXI version 4.

Resolution:
This can be edited in VMware and changed to allow more cores.

Shut the vm down.
Right click the VM in vsphere.
Go to Compatibility --> Upgrade Compatibility
conmpatibility_menu.PNG

You will get a warning stating that this is an irreversible operation. Hit yes.
compatibility_warning.PNG

Choose the last one in the "Compatible With" list and hit OK
compatible_with.PNG

You should now be able to set over 8 CPUs for the DCE 7.9.2
compatible_edit_settings.PNG



***Please note that if you have deployed a version and increased the number of cores, then upgraded that version to the next (not a fresh VM deployment), you will not see this issue.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: