Why the HMI variable parameter of the eCRA device_ddt on M580 HSBY is getting selected automatically at a build ?
Context:
On a control expert project setting with "Embedded data" for datadic with "HMI Only" enable,
When a ECRAis created, the option “HMI Variable” is selected on the device_ddt properties automatically. If this option is unselected, during a build, this option is reselected automatically.
Some customer doesn't want to have those variables inside the datadic.
device ddt ecra

To not have this “HMI variable” selected, the following step need to be follow before performing a build :
workaround

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: