MACHA driver, the Authentication configuration window not displayed correctly.

Issue:
In Machine SCADA Expert, the Authentication configuration window is not displayed correctly for the MACHA driver.

Screenshot of Problem


Product Line:
EcoStruxure Machine SCADA Expert 2020 SP2, MACHA driver.

Resolution:
We saw something similar after changing the display fonts scaling to something different than 100%. So please, set the Scale option for the display to 100% in Windows:

Screenshot of Solution

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: