Can you connect the ATV600 and ATV900 HMI VW3A1111 to the Ethernet network?

Issue:

HMI VW3A1111 directly to the Ethernet network?

Product Line:

ATV600 and ATV900

Environment:

All

Cause:

Wants to connect the remote HMI to the Ethernet network.

Resolution:

No, the VW3A1111 remote HMI cannot be connected directly to the Ethernet network.

The remote HMI or Graphic Display Terminal is only compatible with the Modbus port built into the drive.  The HMI modbus settings baud 19.2k format 8E1

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: