Default IP address, username and password for the Easy UPS 3S NMC (DA807)

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Default IP address, username and password for the Easy UPS 3S NMC (DA807)

Product line:
Easy UPS 3S, every other product using the NMC “DA807”

Environment:
All models, all serial numbers

Cause:
Default IP address, username and password for the Easy UPS 3S NMC (DA807)

Resolution:
The NMC DA807 comes with the IP address 192.168.5.105 by default, you’ll need to change your computer IP to be in range with the NMC IP to be able to connect to it. Open any web browser and type the IP address using HTTPS, once you see the login screen use “administrator” for username and password. In the web interface you’ll be able to change the NMC IP or activate DHCP.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: