Would like to use Machine Expert to program small IFM model CR7032 controller.

Issue:

I have a small IFM CR7032 controller that uses Codesys for its programmation.

Since the EcoStruxure Machine Expert software also uses Codesys to program the Schneider controllers, would it be possible to use it to program this IFM CR7032?

Product Line:

EcoStruxure Machine Expert (all versions)

Resolution:

EcoStruxure Machine Expert does not support controllers other than those from Schneider Electric. So the software will not allow to program an IFM CR7032 controller.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: