EcoStruxure Machine SCADA Expert v2020 SP3 - Modifying background color of Alarm object crashes the application.

Issue:

In EcoStruxure Machine SCADA Expert v2020 SP3, place an alarm object on the screen and click to change the background color. Select a color from the Standard Colors pallet and the software will crash and display the below message.

Crash Error Message

Interestingly enough, if you click the Edit Custom Colors, and chose a color from that pallet, it does not crash the software.

Customer work around

Product Line:

Specific to EcoStruxure Machine SCADA Expert Version 20, Service Pack 3.

Resolution:

This is a known issue on this specific version.

Please check the attached HotFix: EMSE 2020.3.00.01

Please check the ReadMe file for installation instruction.

Schneider Electric Việt Nam

Phần đính kèm
EMSE 2020.3.00.01.zip [1.11 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: