What is the part number for the EcoStruxure Automation Expert Altivar ATV dPAC Module?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Part number for the EcoStruxure Automation Expert Altivar ATV dPAC Module


Product Line:
EcoStruxure Automation Expert,  Altivar ATV


Resolution:
The ATV dPAC module is intended to be used as slide in dPAC option for the Altivar ATV600, ATV900 and ATV340 Variable Speed Drive (VSD) families .
The Altivar ATV dPAC Module is powered by the drive and provides dual Ethernet sockets for connection to peer controllers, distributed IO or remote secondary devices.
The part number is VW3A3530D

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: