DCE 7.9.3 Communications to an SNMP version 3 device may fail if new passphrases are used.
Issue:
Communications to an SNMP version 3 device in DCE 7.9.3 may fail if new passphrases are used.

Product Line:
Data Center Expert (DCE)

Environment:
Data Center Expert 7.9.3
Potentially any SNMP version 3 device.

Cause:
If you change the SNMP version 3 passphrases for an SNMP version 3 device that is already discovered in DCE, even if you change the SNMP parameters in DCE, you may lose communications and not regain it.

Similarly, if you discover and delete a device, then try to discover with changed SNMP parameters, the device may not properly discover or communicate.

Resolution:
It has been seen that the SNMP parameters are being held in the SNMP daemon and a reboot of the DCE system will clear the old parameters out.

If you have changed passphrases on a device and lost communications within DCE even after updating the passphrases there to, a simple reboot of the DCE server should resolve the communications issue.

This issue should be resolved in an up coming revision of Data Center Expert

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: