How can I resolve Error 1722 when installing EcoStruxure Control Expert v15.3?

Issue

Seeing this error when installing.

256938_img

Resolution

  1. Shorten the PC name to less than 15 characters
  2. Restart the PC
  3. Re-install EcoStruxure Control Expert v15.3
  4. Insure you can launch EcoStruxure Control Expert v15.3 Classic or Topology Manager
  5. Change the PC name back to its original length
  6. Restart the PC
  7. Insure you can launch EcoStruxure Control Expert v15.3 Classic or Topology Manager


If you continue to have issues installing EcoStruxure Control Expert v15.3, please contact support either VIA chat from www.se.com, email customer.services@se.com or call 888-266-8705.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: