Power Tags M250/M630 active energy delivered incorrect value in PaS FW 1.5.1 web page
Issue
Power Tag sensors M250/M630 active energy delivered value issue in PaS FW 1.5.1 web page.

Product Line
Power Tag M250/M630
PaS 600/800
PME/EPO

Environment
Power Tag NSX M250/M630 FW 001.001.001 & FW 001.003.003
PaS 600/800 FW 001.005.001

Cause
Power Tag sensors M250/M630 active energy delivered values are out of scale by 1000 in PaS FW 1.5.1 web page.

Resolution
This issue is fixed in latest Firmware 001.006.000. Recommended to upgrade the FW of PaS to 001.006.000.


NOTE:
This issue is not seen in PaS earlier FW 001.004.000. This is present only in FW 001.005.001.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: