How to view Momentum Web pages using Edge.
To be able to view the Momentum Web pages you first need to open Edge (will not work with anything other browser).
1. click on the ellipsis (the 3 dots ... in the top right hand corner)
2 open settings
3. open default browser
4.Internet Explorer compatibility change from Default to Allow
5. Internet Explorer mode pages select ADD and enter the IP addresses of the Momentum's to be viewed
6. Open browser and enter the IP address of the Momentum you want to access Web pages
7. You will now be in Internet Explorer mode
8. you can now select the different options on the Web page.
9. In this example is in monitoring mode, Data viewer,
10. You will receive a popup for Java out of date  select later or do not ask again.
11. Java popup  select I accept the risk and want to run this application.
12. For the Data viewer you can start animation and see the data change.
13. You can then select Diagnostics and select the different options. Status, Ethernet I/O scanning, messaging bandwidth, and statistics.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: