Can EcoStruxure Terminal Expert trial version be used to load a sample project to an HMI?

Issue:

Is it possible to download a project to a physical HMI using EcoStruxure Operator Terminal Expert with the Trial license?

Product Line:

EcoStruxure Operator Terminal Expert (all versions)

Resolution

The trial license for EcoStruxure Operator Terminal Expert has 2 limitations:

1- It is valid for a period of 42 days.

2- It is not possible to download a project to a physical HMI. It can only transfer a project to the simulator.

To transfer to a physical HMI, a Basic or a Professional license is required.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: