Issue:
J751 and J752 connectors on the ATV58 Drives interface board.
Product Line:
ATV58 HHP Drives only.
Environment:
All
Cause:
Voltage measurements
Resolution:
The J751 and J752 connectors on the ATV58 HHP interface board.
J751= L1 L2 L3 line voltage from the Drives main input terminals.
J752= DC bus voltage from the + and - DC bus terminals internal on the drive.
Đã phát hành cho:Schneider Electric Việt Nam