How do you remove the main control boards on the Altistart ATS480 soft starter?

Issue:

Removing the ATS480 Soft Starters main control board.

Product Line:

ATS480

Environment:

All

Cause:

Main control board replacement

Resolution:

Before starting make sure you have removed all the main and control voltage from the ATS480 soft starter before beginning.

Remove the front control terminals cover. (Make sure the door is 90 degrees and push out on the top corner of the cover.)

Now remove the two screws at the bottom of the main control board and lift it up.

Reinstalling you will do in reverse operation.

Main control board picture 1

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: