ATV6000 MV Drive support Ethernet TCP-IP and Ethernet IP?

Issue:

ATV6000 Embedded Ethernet support both Ethernet TCP-IP and IP?

Product Line:

ATV6000

Environment:

All

Cause:

Ethernet Commnications.

Resolution:

Yes, the Embedded Ethernet on the ATV6000 MV Drive does support both Ethernet IP and Ethernet IP.

Note this Ethernet port needs to be configured during the ATV6000 MV commissioning or start up.

Related information

ATV6000 Embedded Ethernet manual link

ATV6000 Ethernet Embedded Manual | Schneider Electric (se.com)

ATV6000 Communications parameters link

ATV600 - Communication parameters addresses Software - Released | Schneider Electric USA

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: