Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
        
Hôm nay chúng tôi có thể giúp gì cho bạn?
In Ecostruxure power commission, What user should do when the see " Application failed to launch " PORT In USE error while launching
1. Go to launch logs by accessing this path in your local computer
C:\Users\SESXXXX\AppData\Roaming\Schneider-Electric\Ecoreach\Logs
                User directory
2. Open EPC EPCLaunchLog.txt logs 
3.Scroll down to view logs with latest date 
4. when user sees logs with text  as shown below : For example 
launch- port in use

5. Node server is not up- which refers , NODE Socket Server port  (8084)is occupied by some other application .
6. To free up the occupied ports , Please refer attached troubleshooting guide (Page -30 to 32) with the help of local IT team.
7. Refer prerequisite for successful installation and launch with the help of local IT team  https://download.schneider-electric.com/files?p_Doc_Ref=DOCA0134EN&p_enDocType=User+guide&p_File_Name=EcoStruxure+Power+Commission+Installation+Guide.pdf

8. Launch Ecostruxure power commission.
 

Schneider Electric Việt Nam

Phần đính kèm
Trouble shooting steps for EPC Launch issue.pdf [2.61 MB]