Issue
Import .eds library
Product Line
Modicon M580
Modicon M340
Modicon Quantum
Environment
EcoStruxure Control Expert
Resolution
Having the ability to have a company or multiple people working on the same project standardize on an .eds library will save time and frustration. To do this you can import a full .eds library into Control Expert. Here are the steps to import the library:
1. Open a Control Expert project.
2. Open the DTM browser
3. Right click on a module, select Device Menu, Additional functions, and Import EDS library.
4. Navigate to where the the exported file is saved.
5. Wait for the import to be successful
Đã phát hành cho:Schneider Electric Việt Nam