Is It possible to update BMENUA0100 firmware via M580 CPU ?
Yes, It is possible to update the BMENUA0100 module firmware via the SERVICE port of the M580 CPU:

1- The module should be on "Secured" mode ( more details here: https://www.se.com/id/en/faqs/FAQ000235297/)

2- A user account with "Installer" role must be created via the module webpage ;

User Management


3-  With EcoStruxure Automation Device Maintenance tool, configure the BMENUA0100 backplane IP address to connect to the module:

IP configuration

4- Use the user account with the "installer" role previously created:

Credentials


5- If it was the first time you connect to the module, It could ask to trust its certificate:

Certificate information

6- Select the firmware to upload:

Firmware selection


7- Launch the update and follow the steps:

Update process
Best Regards.





Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: