Access to SC&LV maintenance webserver using http://192.168.10.10
Answer:
This access is used for example when changing module's IP address or upgrading firmware.
Always make sure that the module's Ethernet connection is isolated from other modules
Still it may not be possible to ping or to connect to http://192.168.10.10 if there has been an IP@ conflict issue.
Please set your Laptop IP as 192.168.10.11
  • Well think to shut down/on the module AFTER having disconnected the Ethernet connections
Afterwards when making modifications, well clear the web explorer cache to refresh the data (F5)
Note also that this access may be disabled during commissioning through T300 webserver as an hardening measure.
Use also T300 webserver to reenable it when relevant for maintenance purpose.
Connect now with http://192.168.10.10

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: