V321 and IO unit maintenance LED on
Issue
Customer found that every now and then the maintenance LED on V321 and I/O unit is on and off.

_____________________________________________________________
Product Line

VAMP321
_____________________________________________________________

Environment
All firmware version
_____________________________________________________________

Root Cause
Please check if the address of VAM4C is 32 or not.
As stated in our manual, address 32 is reserved for Master Unit, and only one device can be set to Master mode in one Arc system, if two masters exist in same Arc system, it will cause some errors in system.
1
2


_____________________________________________________________

Solution
Set the address of VAM4C to another address except 32 and install the system again.
3

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: