How to Invert the CT polarity of an ION Meter that does not have the Verification tab in the Setup Assistant
Issue
Some ION meters do not have the Verification tab in the Setup Assistance due to age making it difficult to understand how to change polarity of CTs

Product Line
ION metering
ION Setup


Environment
ION Setup

Resolution
The attached documents details the steps required to change the polarity of an ION meter

Schneider Electric Việt Nam

Phần đính kèm
How to Invert the CT polarity of an ION Meter that does not have the Verification tab in the Setup Assistant (1).pdf [207.56 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: