In Ecostruxure Power commission , What user should do when upgraded firmware version in not reflecting in report after successful firmware upgrade?
Follow these steps.
1. Start a fresh project
2.     Rediscover the same device
3.     Add device
4.     Generate report
The version of the firmware will be updated in the project report.

Schneider Electric Việt Nam