Firmware / Hardware compatibility for Lexium 62 devices
Definitions:
Lexium 62 Standard
Lexium 62 Standard Plus: Successor device for LXM62 Standard with additional features
Lexium 62 Advanced Plus: New device based on LXM62 Standard Plus with additional features

The Lexium 62 Standard and the Lexium 62 Standard Plus have the same commercial reference, however, they can be distinguished by the revision number and the QR code on the front cover.

Hardware/firmware compatibility list:
Device typeCommercial ReferenceHW RevisionQR code on the front of the deviceCompatible firmware
Lexium 62 StandardLXM62DxxxC
LXM62DxxxD
RS0xNoV01.32.xx.xx - V01.54.xx.xx
Lexium 62 Standard SafetyLXM62DxxxE
LXM62DxxxF
RS0xNoV01.54.xx.xx
Lexium 62 Power Supply StandardLXM62PRS0xNoV01.32.xx.xx - V01.54.xx.xx
Lexium 62 Standard PlusLXM62DxxxC
LXM62DxxxD
RS1x and higherYesV01.36.12.xx - current FW *
Lexium 62 Standard Plus SafetyLXM62DxxxE
LXM62DxxxF
RS1x and higherV01.54.xx.xx – current FW *
Lexium 62 Advanced PlusLXM62DxxxGRS1x and higherYesV0.1.60.xx.xx - current FW
Lexium 62 Advanced Plus SafetyLXM62DxxxHRS1x and higherV01.60.01.xx – current FW
Lexium 62 Power Supply Standard PlusLXM62PRS1x and higherYesV01.36.12.xx –
V01.54.xx.xx
*The new functions can only be used from FW V01.60.xx.xx onwards.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: