Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
        
Hôm nay chúng tôi có thể giúp gì cho bạn?
How do I mute the sound or alarm for APC Back UPS Floor/Wall mount such as BE1050G3,BE900G3,BE700G3 and BE500G3?


Issue:  How do I mute the sound or alarm for APC Back UPS Floor/Wall mount such as BE1050G3,BE900G3,BE700G3 and BE500G3?

Product Line: BE1050G3,BE900G3,BE700G3 and BE500G3

Resolution:  UPS models BE1050G3,BE900G3,BE700G3 and BE500G3  can mute and unmute using the small button located at the side panel of the UPS.

See simple instructions below:

1. Press and hold the small button until the beep was heard and the LED green will illuminate (alarm is muted/disabled).
2. Press and hold again the small button until the beep was heard and the LED Green will turn off (alarm is unmuted/enabled)

Muting the Mt Bona.JPG

NOTE: UPS models BE1050G3 and BE900G3 is capable of connecting to PCSS (PowerChute Serial Shutdown) because it has a USB port. Through PCSS there is an option for the 2 mentioned UPS models to disable (muted) and enable (unmuted) the alarm.
See image below (showing the procedures);

Step 1 ; From PCSS, Go to product decription and click "UPS settings".
Step 1 A.JPG

Step 2:  From Audible section, you can choose it's either "Disable or Enable".

Step 2 muting.JPG

Step 3: After setting up or choosing the alarm condition whether disable or enable, don't forget to click or hit "Apply" to activate the current set-up.

step 3 muting.JPG

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: