{}

Nhãn hiệu của chúng tôi

Chào mừng bạn đến với Trang web của Schneider Electric

Chào mừng đến với trang web của chúng tôi.
Tìm các câu hỏi thường gặp
How to change the PowerChute Network Shutdown license from trial to full?
Issue:
Would like to activate a PowerChute license after running PowerChute in trial mode.

Product:
PowerChute Network Shutdown version 5.1

Environment:
All supported OS that require licensing

Cause:
Informational

Solution:

Log in to the PowerChute web UI and navigate to Configure > PowerChute Setup.
PowerChute setup menu

Once the setup wizard has started, navigate to the PowerChute License Setup page.
PowerChute license setup page
Select Activate Online, Activate Offline, or Local Licensing Server.

Enter the license activation code and select Activate.
Activate the license
For assistance with activating a license offline, see Schneider Electric FAQ000264494.

For assistance with activating via the local license server, see the attached PDF Local License Server Activation.

Schneider Electric Việt Nam

Phần đính kèm
Local License Server Activation.pdf [1.08 MB]