What is the max depth of the APC Smart-UPS 4 Post Rail Kit?
Issue:
What is the max depth of the APC Smart-UPS 4 Post Rail Kit?

Product Line:
Smart-UPS 4 Post Rail Kit

Environment:
SU032A, SURTRK, SURTRK2, SRTRK2, and SRTRK4

Cause:
A customer wants to know what is the max depth or how long they can extend a 4 post rail kit

Resolution:
The noted rail kit mounting rails can be physically extended up to 36 inches (91.44cm).

However, please be aware that a cabinet's vertical mounting rails may have tolerances. You may also need to adjust the depth of the vertical mounting rails of your cabinet for proper fitment. For APC NetShelter cabinets, please refer to the Installation and Customization Manual. For 3rd party cabinets, please contact the cabinet manufacturer for more info.

Please take note that these SKUs comes with different accessories depending on the model of the Smart-UPS. Always double check which is compatible for your Smart-UPS model.

Should there be any further concerns, please contact our Customer Care Center at https://www.apc.com/us/en/support/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: