NetBotz 5.4 upgrade error "Firmware update failed because of invalid signature (40)"
Issue:
NetBotz 5.4 upgrade error "Firmware update failed because of invalid signature (40)"

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755
NetBotz 5.4 firmware

Cause:
Prior versions of NetBotz 750/755 firmware allowed you to upgrade from any version to the most current. This is changed for 5.4. You will receive an error of "Firmware update failed because of invalid signature (40)" if attempting to upgrade from 5.3.4 or prior.

Resolution:
The NetBotz 5.4 update requires that the NetBotz appliance be at version 5.3.5 to work. If you're seeing the above error, make sure you update to 5.3.5 prior to upgrading to 5.4

Please check release notes for upgrade information as well as any future version requirements.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: