Side by Side Configuration error is incorrect on SCADAPack E configurator

Problem:

The application failed to start because its Side-by-Side configuration is incorrect. Please see the application event log or use the command-line sxstrace.exe tool for more derails.

sIDEBYSIDE2

using windows event viewer>windows logs>applications; to view events that have occurred on your computer.

If the error indicates Dependent Assembly Microsoft.VC80.MFC,processorArchitecture="x86",publicKeyToken="1fc8b3b9a1e18e3b",type="win32",

version could not be found.

Sidebyside1

Follow the steps below:

  • Uninstall the SCADAPack E configurator.
  • Install the C++ 2005 redistributable using the link below.

https://www.microsoft.com/en-us/download/details.aspx?id=26347

  • Re install the SCADAPack E configurator.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm:
Phạm vi: