Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Schneider Electric releases solar solutions that provide clean power to communities with limited access to energy

Rueil-Malmaison, France

28/06/2022

Download PDF
  • Two new solar power solutions launched at the Alliance for Renewable Energy’s flagship event in Tanzania
  • Supporting long-term commitments to provide access to clean electricity to 100 million people by 2030

Schneider Electric, the leader in the digital transformation of energy management and automation, which was named the world’s most sustainable corporation by Corporate Knights Global 100 Index in 2021, today announced the launch of two new solar power solutions for communities that have little or no access to energy.

The new solar products are designed to withstand extensive use for a wide range of power needs. They expand Schneider’s portfolio of products and solutions that aim to help reach the United Nations’s 2030 target of universal access to energy.

According to the World Bank, 733 million people worldwide still have no access to electricity. Africa’s population remains the least electrified in the world: 568 million people across the continent lack electricity access.

“Aligned with the UN’s Sustainable Development Goals, Schneider Electric is committed to having a positive impact on our many stakeholders, especially when it comes to addressing climate change and social inequality,” said Carol Koech, Schneider Electric’s Country President for East Africa. “Our energy efficient products and solutions are designed to help communities that live in locations where the grid is either unreliable or non-existent.”  

The product launch coincided with the Alliance for Rural Electrification’s (ARE) Energy Access Investment Forum 2022 in Dar es Salaam, Tanzania, from 28-30 June, where representatives from the public and private sectors, including Schneider Electric, are meeting as part of ongoing active support to achieve a sustainable energy future for all.

Schneider’s new products are now commercially available worldwide.

Homaya Pro powers off-grid communities with reliable, affordable and green electricity

The new Homaya Pro solar-hybrid inverter converts direct current electricity to alternating current to be used in stand-alone systems or connected to a grid. It can power the energy needs of a household or a small business, with solutions ranging from 3, 4 or 6 kilowatts. It provides reliable renewable energy access for homes, fuel stations, small offices, healthcare centers, schools and telecommunications infrastructure.

ta26mjekf6-phpyctzhi

The Homaya Pro inverter is powered by solar energy with an inbuilt Maximum Power Point Tracking (MPPT) controller. It is compatible with grid charging and supports lead or lithium battery technologies. Up to 6 inverters can be connected in parallel for a combined output of up to 24 kilowatts. Optional accessories include external MPPT to extend a solar array by one or three kilowatts and increase backup capacity, and a WiFi dongle to allow local internet monitoring without a mobile app.

Mobiya Original solar lanterns for lighting and mobile charging

The latest Mobiya Original solar lantern provides users with safe, reliable and clean energy for lighting and USB charging needs. Based on the robust and waterproof Mobiya Original lantern, this upgraded version incorporates new design features and improvements that make it easier to handle and use.

1xzulcwz9a-phpt0rgcq

Made from recyclable materials, this latest version produces 280 lumens and includes settings to save power and prolong lighting performance over time.

“Launching these new offers demonstrates Schneider Electric’s commitment to ensuring that 100 million people will have access to green energy by 2030”, said Olivier Jacquet, Schneider Electric’s Vice President for Access to Energy Business Development in the Middle East and Africa. “Homaya Pro is not only easy to use and install but also affordable for people living in remote parts of Africa and Asia.”

Since launching its Access to Energy program in 2009, Schneider Electric has been developing and commercializing safe, affordable and reliable technology solutions to harness more renewable power, improve the lives and livelihoods of people often located in remote places, and support the growing energy needs of developing countries.

Adoption of Wiztopic's Blockchain Certification Platform

From October 2nd, 2019, in order to secure its communication, Schneider Electric certifies its contents on Wiztrust. You can check the authenticity on the website Wiztrust.com for Corporate communications.
View press release (pdf, 185 kb) opens in new Window
Share this page: