Search FAQs
How do you set the ATS48 softstarter for a Heavy (Severe) Duty Application?
Issue:
ATS48 setup for a Heavy Duty or Severe Application
Product line:
Altistart 48, ATS48 soft start
Environment:
all
Cause:
Rating guide shows Normal and Severe (or Heavy Duty)
Resolution:
There is no switch or setting to designate ``Heavy Duty``
Oversize the ATS48 selection by one size, based on the motor FLA rating. For example, for a 50HP @ 460V, select the 60HP size.
In addition to the default Programming, set the overload class (PRO > THP ) to 20.
ATS48 setup for a Heavy Duty or Severe Application
Product line:
Altistart 48, ATS48 soft start
Environment:
all
Cause:
Rating guide shows Normal and Severe (or Heavy Duty)
Resolution:
There is no switch or setting to designate ``Heavy Duty``
Oversize the ATS48 selection by one size, based on the motor FLA rating. For example, for a 50HP @ 460V, select the 60HP size.
In addition to the default Programming, set the overload class (PRO > THP ) to 20.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: