{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there a 9001 KA contact block that is rated 6A at 125VDC?
Issue:
9001KA contact rating

Product Line:
9001 Type K Heavy Duty Operators

Environment:
30 mm Push Buttons

Resolution:
No., the 9001KA contact blocks have a maximum of 2.5A continuous at 125VDC.

Schneider Electric Global