{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Will the display still be active if a ModBus network is attached to the ATS48 or ATS22?

Issue:
Is the integrated display active when ModBus Network is attached to ATS48 or ATS22.

Product Line :
Altistart Soft Starters

Environment:
Open style Soft Starters

Cause:
Communication

Resolution:
The ATS48 and ATS22 soft starters have a built in display as part of the soft starter. The RJ-45 port can be used for a remote mounted display keypad or for Modbus network. If the RJ-45 port is used for communications or for remote keypad the local display on the soft starter control board will still operate.

The single available port cannotbe used for both a remote keypad and for Modbus communication unless you add a port expander which allows for 2 Modbus Network Masters.  Schneider Electric does not offer and expander, so this would require a 3rd party product.  Another option is to monitor the motor using a TeSys T.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: