Search FAQs
What is the power board part number for the Altivar ATV58 drive?
Issue:
Power board part number for the Altivar ATV58 drive.
Product Line:
Altivar ATV58, Flex58 58M,58E
Environment:
All
Cause:
Replacement power board part numbers for the ATV58 drives.
Resolution:
All parts above are limited and *field service parts have to be installed by field services. | |||
*Any parts of Altivar 58 or FLEX58 is no longer available. Only option is to replace the drive.* |
Released for:Schneider Electric Global
Explore more
Range:
Category:
Explore more
Range:
Category: