Issue:
Do we have fingersafe covers for the 9422ATF11, 9422ATF12, 9422ATF13 or 9422TG Operating mechanisms?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Disconnect Switches
Resolution:
No. Barriers are currently only available up to the 100A mechanism, 9422TE.
Do we have fingersafe covers for the 9422ATF11, 9422ATF12, 9422ATF13 or 9422TG Operating mechanisms?
Product Line:
Operating Mechanisms and Disconnect Switches
Environment:
9422 Disconnect Switches
Resolution:
No. Barriers are currently only available up to the 100A mechanism, 9422TE.