Search FAQs
What is the part number for door screws on the E-Flex drives?
Issue:
Part number for door screws on the E-Flex drives
Product Line:
ATV61
Environment:
Econo-Flex
Cause:
n/a
Resolution:
The door screw for the E-Flex will fit the Econoflex as well. There is also a retaining washer that is useful to have.
The part numbers and pricing are as follows per Pam Welborn in Seneca.
22906-00003 Screw - Thumb, Stainless $29.52 List Price PE4 Discount
29416-61501 Washer - Retaining $1.00 List Price PE4 Discount
Need to force the order on Seneca.
Part number for door screws on the E-Flex drives
Product Line:
ATV61
Environment:
Econo-Flex
Cause:
n/a
Resolution:
The door screw for the E-Flex will fit the Econoflex as well. There is also a retaining washer that is useful to have.
The part numbers and pricing are as follows per Pam Welborn in Seneca.
22906-00003 Screw - Thumb, Stainless $29.52 List Price PE4 Discount
29416-61501 Washer - Retaining $1.00 List Price PE4 Discount
Need to force the order on Seneca.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: