Search FAQs
Can your InRow Cooling Auto-Start after a Power Failure
Issue:
Can your InRow Cooling Auto-Start after a Power Failure
Product line:
InRow
Environment:
Data Center Cooling
Cause:
Resolution:
The InRow RC, RD, RP and SC will start automatically if the power is restored after a power failure. The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state.
It is also possible to configure a Start up Delay of 0 to 999 seconds.
That can be done from:
Can your InRow Cooling Auto-Start after a Power Failure
Product line:
InRow
Environment:
Data Center Cooling
Cause:
Resolution:
The InRow RC, RD, RP and SC will start automatically if the power is restored after a power failure. The unit will go to its last known state, ie if the unit was in standby, the unit would return to standby, or if the unit is on, the unit would return to the on state.
It is also possible to configure a Start up Delay of 0 to 999 seconds.
That can be done from:
- The Display: Configure Unit>General> Startup Delay
- The Network Management Card Interface: Unit>Unit Configuration> Startup Delay
Released for:Schneider Electric Global
Explore more
Product:
Explore more
Product: