Search FAQs
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Issue:
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Product Line:
NetBotz
Pelco Cameras
Environment:
NetBotz NBWL0455 and NBRK0570
4.X botzware
Pelco camera support
Cause:
Not all Pelco cameras have been tested with NetBotz 4.0 botzware.
Resolution:
Please note that the NetBotz 3xx and NetBotz NBRK0450/0451 do not support the Pelco integration.
The initially supported Pelco cameras from version 3.x firmware are:
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.0. The Sarix line of Pelco cameras have been added to testing:
With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested:
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.4:
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.3:
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.6.3:
Important Note:
Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.
Models of Pelco cameras that have been tested with version 3 NetBotz and BotzWare 4.X
Product Line:
NetBotz
Pelco Cameras
Environment:
NetBotz NBWL0455 and NBRK0570
4.X botzware
Pelco camera support
Cause:
Not all Pelco cameras have been tested with NetBotz 4.0 botzware.
Resolution:
Please note that the NetBotz 3xx and NetBotz NBRK0450/0451 do not support the Pelco integration.
The initially supported Pelco cameras from version 3.x firmware are:
Pelco Camera Model | Product Family | Firmware Version Tested |
IP3701H-2 | IP | Unavailable |
IP110-CHV9 | IP110 Camclosure® | Unavailable |
SD4N-W0 | Spectra Mini IP | Unavailable |
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.0. The Sarix line of Pelco cameras have been added to testing:
Pelco Camera Model | Product Family | Firmware Version Tested |
IXS0C | Sarix IX | 1.7.19.9080-A1.5842 |
IXE20DN | Sarix Enhanced | 1.7.19.9081-A1.5843 |
IX30DN | Sarix IX | 1.7.8.9080-A1.5288 |
IMSOC10 | Sarix IME | 1.7.41.9260-O2.6725 |
SD4N-W0 | Spectra Mini IP | 1.2.15 |
With the release of Botzware 4.2, the following list of additional Pelco cameras and firmwares have also been tested:
Pelco Camera Model | Product Family | Firmware Version Tested |
IMSOC10 | Sarix | 1.8.2 |
IM10C10 | Sarix | 1.8.2 |
IX30DN | Sarix IX | 1.8.2 |
D5118 | Spectra HD | 1.8.2 |
TXB-N | Spectra IV IP | 1.8.2 |
DD4N-W0 | Spectra Mini IP | 1.2.15 |
IP110 | IP110 Camclosure® | 1.0.47 |
IP3701 | IP | 1.0.10 |
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.4:
Pelco Camera Model | Product Family | Firmware Version Tested |
---|---|---|
IM10C10 | Sarix | 1.9.2 |
IMS0C10 | Sarix | 1.9.2 |
D5118 | Spectra HD | 1.9.2 |
IME119 | Sarix Enhanced | 2.1.2.0.8280-A0.0 |
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.5.3:
Pelco Camera Model | Product Family | Firmware Version Tested |
IL 10 | Sarix | Unavailable |
The following is a list of cameras and Pelco firmware that has been tested with BotzWare version 4.6.3:
Pelco Camera Model | Product Family | Firmware Version Tested |
IJP121-1IS | Sarix | 1.16.37 |
Important Note:
Pelco Sarix Pro models that were originally listed as supported do not correctly update the resolution settings presented to NetBotz appliances. NetBotz can no longer support Sarix Pro models due to this limitation of the Pelco camera and they have been removed from this compatibility matrix.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: