{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

How are the Color Codes 568A and 568B different?

Issue:
The difference between T568A and T568B color codes is needed.

Product Line:
Cables and Connectivity Solutions, Patch Panels

Environment:
CAT6PNL-24 and CAT6PNL-48, all serial ranges.

Cause:
Not following the correct color code can cause wiring errors.

Answer:
568A and 568B are color code standards that show which color wire matches up with a specific position on an RJ45 connector. When designing a network infrastructure only one color code can be followed. All commercial and residential wiring in the US follows TIA 568B color code.

T568B Color Code
RJ45 Pin---Pair Color
1-------------White/Orange
2-------------Orange
3-------------White/Green
4-------------Blue
5-------------White/Blue
6-------------Green
7-------------White/Brown
8-------------Brown

T568A Color Code
RJ45 Pin---Pair Color
1-------------White/Green
2-------------Green
3-------------White/Orange
4-------------Blue
5-------------White/Blue
6-------------Orange
7-------------White/Brown
8-------------Brown

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: