{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Is there a roof available for the AR3100 which is solid and does not have open cable access holes?

Issue:
There may be a need for a solid roof on the cabinets.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
A more secure roof may be required for installations such as PCI.

Resolution:
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.

Schneider Electric Global

Attachment(s)

20131206 WAR7210 High Security Roof.pdf20131206 WAR7210 High Security Roof.pdf [20.32 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: