{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is there information available regarding EIA-310-D, EIA/ECA-310-D and EIA/ECA-310-E?
Issue:
Clarification is needed on the various EIA 310 governing bodies.

Product Line:
NetShelter SX, NetShelter VX, NetShelter WX, NetShelter SV

Environment:
All versions and serial ranges.

Cause:
The EIA 310 organization has changed specification and owners in the past several years. What is the difference between these governing bodies?

Resolution:
See attached file

Schneider Electric Global

Attachment(s)
20120402 EIA-310-D ECA-310-D Info Rev2.pdf [45.74 KB]