Search FAQs
How much exhaust clearance is needed for a NetShelter CX cabinet?
Issue:
The NetShelter CX may overheat if there is not proper clearance for airflow.
The NetShelter CX may overheat if there is not proper clearance for airflow.
Product Line:
NetShelter CX
NetShelter CX
Environment:
All models and serial ranges.
All models and serial ranges.
Cause:
Improper spacing can cause overheating.
Improper spacing can cause overheating.
Resolution :
See attached file.
See attached file.
NetShelter CX Wall Clearance
The exhaust fans of the NetShelter CX vent to the sides. The back of the cabinet can be placed against a wall if desired.
If the cabinet is being installed in a corner please leave at least 6 inches of open space between the side of the NetShelter CX and the wall.
It is not recommended to install a NetShelter S X where the back and both sides are against a wall.
Please see attached file for a graphic depiction of the clearance.
Please see attached file for a graphic depiction of the clearance.
Released for:Schneider Electric Global
Attachment(s)
Explore more
Range:
Explore more
Range: