Search FAQs
Will my APC Back-UPS Automatically restart following the return of utility power?
Issue:
Will my APC Back-UPS Automatically restart following the return of utility power?
Product Line:
All APC Back-UPS
Environment:
All APC Back-UPS
Cause:
When the UPS runs on battery operation and the battery becomes discharged, the UPS automatically switches off.
Resolution:
Yes, when adequate power is restored to the UPS and is within the operating voltage range of the UPS, it will restart in online operation.
This is independent with PowerChute software either installed or not. An attached computer may also be configured to restart following a complete discharge of the UPS, which has resulted in the UPS turning off.
On the other hand, the computer may not wakeup/restart automatically.
The computer must have the option for powering on when power is available, chosen in the systems BIOS for this work. See Kbase FA159550 for information concerning BIOS settings.
Note: The UPS will continue to recharge its battery in the Off state, as long as there is some voltage present on the electrical circuit.
Will my APC Back-UPS Automatically restart following the return of utility power?
Product Line:
All APC Back-UPS
Environment:
All APC Back-UPS
Cause:
When the UPS runs on battery operation and the battery becomes discharged, the UPS automatically switches off.
Resolution:
Yes, when adequate power is restored to the UPS and is within the operating voltage range of the UPS, it will restart in online operation.
This is independent with PowerChute software either installed or not. An attached computer may also be configured to restart following a complete discharge of the UPS, which has resulted in the UPS turning off.
On the other hand, the computer may not wakeup/restart automatically.
The computer must have the option for powering on when power is available, chosen in the systems BIOS for this work. See Kbase FA159550 for information concerning BIOS settings.
Note: The UPS will continue to recharge its battery in the Off state, as long as there is some voltage present on the electrical circuit.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: