{}

Welcome to the Schneider Electric corporate Website

Search FAQs
Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.

Issue:
Missing native shutdown battery options in Windows

Product Line:
Back-UPS and Smart-UPS

Environment:
Microsoft Windows 7, 8, 10, 11

Microsoft Server 2008, 2010, 2012, 2016, 2019, 2022, 2025

Cause:
When viewing Power Options (go to Control Panel—Power Options), you may find that the configurable battery shutdown options are missing or unavailable. This may be caused by the HID driver (Human Interface Device) being updated from HID UPS to APC UPS or APC Battery Back-UPS.

Solution:
If you no longer use PowerChute software and want to utilize native battery options, you may need to roll back / revert the HID Driver to HID UPS.
The featured video explains how to revert/restore the HID UPS Driver, which will allow for the configuration of the native battery shutdown option.
For information on how to configure Windows 7, 8, 10, 2008, 2010, Server 2012, 2016, 2019, 2022, and 2025 to safely shutdown without using APC's PowerChute software, please review the FAQ Configuring Microsoft Windows 7, 8, 10, & 11 Windows Server 2008, 2012, 2016, 2019, & 2022 to safely shutdown without using APC's PowerChute software.

Schneider Electric Global

Video: What to do if the system is missing native shutdown battery options / How to restore HID UPS device driver.

Issue:
Missing native shutdown battery options in Windows

Product Line:
Back-UPS and Smart-UPS

Environment:
Microsoft Windows 7, 8, 10, 11

Microsoft Server 2008, 2010, 2012, 2016, 2019, 2022, 2025

Cause:
When viewing Power Options (go to Control Panel—Power Options), you may find that the configurable battery shutdown options are missing or unavailable. This may be caused by the HID driver (Human Interface Device) being updated from HID UPS to APC UPS or APC Battery Back-UPS.

Solution:
If you no longer use PowerChute software and want to utilize native battery options, you may need to roll back / revert the HID Driver to HID UPS.
The featured video explains how to revert/restore the HID UPS Driver, which will allow for the configuration of the native battery shutdown option.
For information on how to configure Windows 7, 8, 10, 2008, 2010, Server 2012, 2016, 2019, 2022, and 2025 to safely shutdown without using APC's PowerChute software, please review the FAQ Configuring Microsoft Windows 7, 8, 10, & 11 Windows Server 2008, 2012, 2016, 2019, & 2022 to safely shutdown without using APC's PowerChute software.

Schneider Electric Global

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
move-arrow-top