Search FAQs
Can a NetBotz HID door handle be used on the AR3200 NetShelter Colocation or NetShelter SV cabinets?
Issue:
NetBotz HID door handles will not latch when used on the NetShelter Colocation or SV cabinets.
Product Line:
NetShelter SX Colocation, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The hasp which ships with the HID door handles will not work on the NetShelter SX Colocation or NetShelter SV cabinets.
Resolution:
Replacement hasps for the NetShelter SX Colocation and SV cabinets are now included with the HID door handle. The original hasp must be removed and replaced.
NetBotz HID door handles will not latch when used on the NetShelter Colocation or SV cabinets.
Product Line:
NetShelter SX Colocation, NetShelter SV
Environment:
All versions and serial ranges.
Cause:
The hasp which ships with the HID door handles will not work on the NetShelter SX Colocation or NetShelter SV cabinets.
Resolution:
Replacement hasps for the NetShelter SX Colocation and SV cabinets are now included with the HID door handle. The original hasp must be removed and replaced.
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: