{}

Welcome to the Schneider Electric corporate Website

Search FAQs
BMS AP9921X-AP9922; alarms “Battery Cell Shorted”
 
 
 
Issue:
BMS AP9921X-AP9922; alarms “Battery Cell Shorted”
 
Product line:
Battery Management System (BMS) AP9921X-AP9922
 
Environment:
All models, all serial numbers
 
Cause:
The sum voltage of the indicated battery is below normal, usually by more than the voltage of one cell. The alarm value is calculated using the following formula: ((#Cells/Batt)-1) x (Vstring) (#Cells/Batt) x (#Batt/String) Example: A normally float-charged 12-V VRLA battery measures 13.5 V at 2.25 Volts per Cell (VPC). If the voltage falls below 11.25 V (2.25 VPC x 5 cells), but is still above 0.5 V, the battery activates the Battery Cell Shorted alarm.
 
Resolution:
Check the voltage reading of the indicated battery. If the alarm is accurate, replace the battery immediately.
 
 

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.